This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: Using default configuration to boot Linux system from USB stick

Part Number: TPS65987D


Hi all,

We have the following use case: ApolloLake SOC and TPS65987D for using in DRD mode. The USB-HS signals routed directly to ApolloLake from USB-C

Our idea is to start Linux from USB stick in production case. I mean in case, when the board contains not programmed SPI-NOR for TPS65987D. Is it possible? If yes, then some other questions to it

As I see the TPS65987D has the default configuration 2

for probably our case

And as I understand we can select the configuration 2 via combination of resistors on ADCIN1 but what should we do with the SPI_MISO? We have now the pullUp on this pin as it is defined i datasheet.

For Usb_Vbus_Detect we wanna use the GPIO14 event and for Usb_OTG_ID the GPIO13 event. Should we implement any pullUps/pullDowns to get the feature for our case running? Will that pullUps/pullDowns not disturb the functionality of TPS65987D when the SPI-NOR not yet flashed and in case when it is already flashed?

Thanks,

Best Regards,

Sergey