Part Number: DS92LV16
Other Parts Discussed in Thread: DS92LX2121, SN65LV1023A, DS92LX2122, SN65LV1224B, DS92LV3221, DS10BR254, DS92LV3222, SN65LVDS116
Hello professional,
In my application I drive multiple led panels connected in series at one time. I am trying to find a solution for reducing the cable count between panels and fpga output(there is nearly 2 meter distance between).From the result of my browsing, I presume a ser/des pair or a serializer and a deserializer would be solution. While digging into the E2E forum I saw a lot of variety of ser/des ,flat link ser/des etc.. Which product or product group will u recommend for my application? And another question is, can I make a cascaded configuration with serializer/deserializer pairs. I have to reduce the cable count which is nearly 90 data line at the moment. I am trying to solve this problem in the least costly way. Please enlighten me on this topic.
I got 5 common signal :(Clock,Lathc,OE,Select1,Select2,Select3) and 15 flat panel group each has indivial 6 signal (R1,G1,B1,R2,G2,B2).
Clock will be operated at least 25 MHz.