Hi team,
Customer would like to use 941A to design two panel application and below picture is their diagram.
So my question is can 941A support this kind of application?
Thanks
And I also share their input data throughput quality for your reference. Accordding to resolutions, it seems we should use FPD-LINK4 solution, am I right?
Any suggestion?
Aspect ratios support shall include, but is not limited to:
o 16:9, 16:10, 3:1
● Resolutions support shall include, but is not limited to:
o 1920 x 1200 pixels
o 3840 x 1080 pixels
o 3840 x 1200 pixels
o 3840 x 2160 pixels
o 3840 x 2400 pixels
● Landscape and Portrait DCSDs shall be supported
● Refresh rates (frames per second) support shall include, but is not limited to:
o 30Hz, 60Hz
● Color depth support shall include, but is not limited to:
o Color depth: RGB888 (24 bit) and RGB (30bit) deep color
● Considering the above color depths, the interface shall support at least the following Pixel Clock:
o 140-160 MHz