Replies: 5
Views: 33
Part Number: TPS25750
Hi,
Could you please review my schematic with the BQ25713 charger?
I'm using them in this mode:
The BQ25713 is connected to an 1S2P battery.
I see two issues with the TPS25750 configuration.
pin10 \i2cs_irq and pin 18 \i2cm_irq should be pulled up to LDO_3V3. This will prevent any IRQ from being triggered before the part has booted.
I do not see any issue with BQ25713, but I do not directly support that part. I suggest that you submit the same schematic to the BQ25713 team for further review by them
In reply to Chuck Branch:
Thanks Chuck.
Please update the TPS25750 datasheet that currently states "Tie to ground if unused" for the I2C IRQ pins.
In reply to 6145095:
I have that in process now.
Since the BQ25792 is available now, would you suggest to use that instead of the BQ25713?
I also have a question regarding the Integrated USB Type-C® power delivery (PD) and charging reference design for 2-4 cell batteries" ref design.
Why are these regulators on the schematic when the VIN_3V3 net can be tied directly to LDO_3V3?
Another thing I noticed was the ref design grounded pin 10 and 18 on the TPS25750. Is that incorrect?