Other Parts Discussed in Thread: TFP401, TFP401A
Hi Community,
I am using TFP401 to convert HDMI to CSI(Camera serial interface) signal. I have attached schematic of hardware. I am using two sabrelite board & this converter. First sabrelite HDMI output is connected to this converter & CSI output of converter is given to other sabrelite board.
Converter uses HDMI cable as power supply to turn on TFP401. when I connect HDMI cable to this converter I got Hot Plug detect interrupt. But transmitter can't able to read any EDID information so it stops HDMI transmission. can you please provide me any dummy EDID or document which I can help me to figure out this problem.
Driver of converter is counting number of HSYNC & VSYNC to calculate resolution. I think if TFP401 is on & it is getting HDMI signal then DE pin should be high & should get HSYNC & VSYNC.
Can I tell me basic steps to verify TFP401 is working.
Thanks In advance,
Pratik