Part Number: DS90UB954-Q1
Hi team,
Several problems are occurring in the system of our customers.
The data sent from the camera module of 953 is being output partway, but Line length error and checksum error occurred and output stopped.
I have 2 questions.
#1
They are saying that they handle CSI long packet data with no packet footer added.
Can systems in 953-954 handle data without PF?
#2
They are setting that FS_MODE is back channel of Port 0 and FS_GEN_MODE is Hi / Lo mode.
However, it seems that both FRAMESYNC_HIGH_TIME and FRAMESYNC_LOW_TIME remain the default 0.
Does LINE_LENGTH_ERR or CKSUM_ERR occur due to this setting?
Best regards,
Tomoaki Yoshida