Part Number: TUSB3410
I thought I was out of the woods with the TUS3410 EEPROM Burner, but I cannot get past a particular step. I am using a Windows 10 machine, and have tried this on a Windows 7 machine. I have installed the software and driver provided on the TUSB3410 web page served up by TI. This includes the driver [sllc428a.zip] and EEPROM Burner [sllc443b.zip]. After rebooting pc, I connect up my design [which has a blank 128K PROM and TUSB3410]. The users guide indicates the TUSB3410 should enumerate as a HID device. On my PC it enumerates as a Serial Port.
My first question. Should I not have installed the driver "TI_WDF_USBUART_SINGLE_DRIVER_V6.7.2.0_WHQL.exe"? Is this why it enumerates as a serial port.
How do I get it to register as a HID device?