Part Number: DS90UB954-Q1
Hi Team,
My customer asked CSI-2 setting for below specific case.
Could you check if below settings are reasonable to have sufficient bandwidth?
<< System requirement >>
1. configuration : CMOS sensor + 953 + 954 (single 953 is connected)
2. streaming data : 1920x1080x60fps, 12bit/pixel (Raw12bit)
--> 1.64Gbps with Blanking rate =1.1
3. max 1.5Gbps for ISP lane
<< DS90UB954 configuration >>
1. For FPDLINK setup for non-synchronous CSI-2 mode
set FPD3_MODE = "00",
REFCLK = 25MHz(from xtal oscillator)
2. For CSI-2 setup
From Table 13, to set CSI frequency less than 1.5Gbps with REFCLK=25MHz,
(1) CSI_PLL_CTL[1:0] has to be set as "00"
(2) IND_ACC_CTL[5:2] = "0111"
(3) IND_ACC_ADDR = 0x08
(4) IND_ACC_DATA[7:6] = "11" (csi pll divider setting = 52)
(5) CSI_LANE_COUNT = "10" (2 lane)
With this setting, I expect 954 has 1.3Gbps x 2 lane capability.
Best regards,
Nobuo