Part Number: TUSB9261
Hi,
My customer is going to have a project with TUSB9261.
The following is the info they provided:
For standard UFI command(or SCSI Commands) defined for USB Mass Storage Class, the bridge IC process them as usual.
But for some specific commands,the bridge IC will pass/get the payload to/from the micro SD Card via 1-bit or 4-bit SDIO interface. (1-bit is enough, but 4-bit better)
The SDIO interface of bridge IC can be implemented by GPIO using software/firmware in this design.
Please help to check :
1. If it is achievable by modifying TUSB9261 FW?
2. Does it have any SW or HW limitation for this application?
Thanks.