Part Number: TPS65987D
Hello,
My customer is trying to configure this part to work in multifunction mode (pass both DP 1.4 and USB 3.0), but we are having some trouble.
In the GUI tool, register 0x51 bit 34 is called out as "Force USB Configuration", but Table 3-62 in the TRM says byte 5 bits 7:1 is Reserved. Perhaps this bit refers to Byte 6 bit 1? It's not clear from the name. We are wondering if this would help enable USB 3.0 and DisplayPort.
Also, when I try to use Debug Mode in the GUI tool, every bit of every register reads back as 1, i.e. Mode (0x3) reads 0xffffffff. We cannot confirm the part is configured as set in the tool.
What would be needed to help diagnose this issue?
Thanks,
Michael