Hi TI.
I am currently evaluating the circuit using the SN75374, but I would like to know about the internal circuit of this IC.
(1) When wiring is performed as shown in the attached circuit diagram SCH1 and the 5V power supply is turned on, pop noise of 1V or more is instantaneously generated at the output terminal Y.
As a boot sequence for this IC, it is necessary to apply the voltage of VCC1 first, and then the voltage of VCC2 and VCC3. Do you agree with me?
(2) After connecting the power supply as shown in the attached circuit diagram SCH2, when observing the terminals of VCC2 and VCC3 with an oscilloscope, the voltage was output. (Unintended voltage)
Why is the voltage output?
I did not find any internal wiring in the data sheet that would output the voltage of VCC1 to VCC2 and VCC3.
(3) As a result of answering (2), since the power supply of VCC1 is applied first in the startup sequence, unintended voltage is momentarily applied to VCC2 and VCC3.
Should the power supply circuits of VCC2 and VCC3 be dedicated circuits that are not used in combination with other circuits?
Sincerly.
YuzuruTI_SCH.pdf