Part Number: AM26C32
Hi,
As known, AM26C32 device is a quadruple differential line receiver for balanced or unbalanced digital data transmission.
Now customer requires compatibility with single-ended input. And we have two ways to meet that.
1、Input A+ connects to single-ended signal, leave pin A- floating.
2、Input A+ connects to single-ended signal, connect the A- through a resistor divider with Vcc.
Obviously, the second method is more reasonable relatively.
But by test, both methods are feasible and the first one performs better.
TI don't provide Pspice model, I cannot do a functional simulation.
So,refer to the functional block diagram below in the datasheet, I do functional simulation with pspice.
The result is puzzling that very different from expectations.
My question :
1、Please help to explain the phenomenon.And which method should be used.
2、For single-ended signals, are there any anti-interference measures?
3、Before, I use a RC filter between A+ and A-,the single-ended signal is greatly affected by RC. Does it have to be removed?
Thanks.