Part Number: SN65DSI86
Hi
My customer has two questions
1. When MIPI DSI1 is not in use, should I float or pull up?

2. EVM line GPIO3 is the function of EDP_BL_ENABLE But REFCLK is set to 27MHz, and GPIO[3:1] requires an external resistor to set 011 But EDP_BL_ENABLE of EVM is pulled LOW directly,
and EVM is also set to 27MHz output Please also help confirm whether the GPIO needs to be pulled LOW