Other Parts Discussed in Thread: DS80PCI102
Hi,
I'm hoping this is a stupid/simple question but here goes. I'm looking at this device DS80PCI102 or similar (possibly the 4 lane) for a PCI Express Gen 2 application. I note that internally it terminates 100Ω differentially and 50Ω singled ended, but my understanding is that for Gen 2 and higher differential routing should be at 85Ω differential, so I would expect the termination to match?
This re-driver will interface with an FPGA where it is possible to configure the termination to 85Ω or 100Ω depending on the application, which ties in with how I would expect a design to work. However the re-driver doesn't have this option.
I don't have access to the PCIe spec currently to check but I thought I would ask the question as to if anyone knows why this is the case?
Thanks,
Alan