Part Number: DS90UB954-Q1
Dear Sir,
Pls advise to check about UB954 BCC_CONFIG(0x58) D[2:0] BC_FREQ_SELECT setting.
Referring to the description on spec, it should be configured to 50Mbps if our serializer is UB953.
But if we initial this register to 0x5e (BC_FREQ_SELECT -- 110 ; 50Mbps ) then we would get trouble to communicate via I2C.
Only setting to 0x5d (BC_FREQ_SELECT – 101 : 25Mbps), and the communicating by i2c is working properly.
Do you know why i2c can’t be working properly if set BC frequency to 50Mbps.
Thanks, Ian.