Part Number: DS90UB949-Q1
Other Parts Discussed in Thread: DS90UB954-Q1,
Hi,
I'm looking towards an application, where I have to source an test image for the DS90UB954-Q1, which is listed under Camera SerDes. Nevertheless I assume, that this chip is compatible with the DS90UB949-Q1 due to the same FPD3 Link interface. Am I correct?
Is my understanding correct, that the maximum resolution of 1080p60 of the DS90UB949-Q1 is only archived, when using both FPD3 link connections together? So In my application, where I only have to source one FPD3 Link signal for the DS90UB954-Q1, it would not be possible to have it going at 60Hz with the DS90UB949-Q1 Serializer as source?
Concerning the Power over Coax, the DS90UB949-Q1 does not mention anything in its datasheet. Still my application would make use of the PoC due to the DS90UB954-Q1 chip. I don't see the reason for the DS90UB949-Q1 to not support the PoC, since I've to filter it prior the chip anyway. Am I missing something here?
Thanks in advance :)