Other Parts Discussed in Thread: DP-EXPANSION-EVM, TPS65982, TPS65981
Tool/software: Linux
Hello all,
Have a question coming in from a customer, let me know if this is able to be answered or needed to brought to the product line's attention.
"I am currently bringing up a TPS65986 USB-C front end for a project.
I have gotten the basic functionality to work for USB 2.0 and 3.0 signaling.
At this time I am trying to get alternate mode working. I have tested the dev board with a DisplayPort dongle to make sure that my configuration is correct. Then I have switched over to another design design.
The design uses USB-C receptacle, and then internally drives a DisplayPort re-timer followed by DisplayPort receiver. The re-timer and receiver were verified to operate when the connection was previously made to thunderbolt port.
when I connect I can see hot plug detect light go on the Ti development board, but no high speed traffic is generated. It looks like the muxes are not configured correctly.
I have attempted to download debug information from our USB-C side, but our I2C address is not at 0x38. Is there a way to change the debug mode setting. I have tried to do it in Debug->Configure I2C/SPI Adapter Settings, but the value for I2C address does not stick."
Please let me know if this able to be answered given the information and I can ask the engineers for more information if necessary.
-Craig