Part Number: SN6505B
Hi team,
Does SN6505 can be designed for output voltage +18V and -3V? thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
Yes, outputs voltages of +18V and -3V are possible with a right transformer design. The total maximum input current will be limited to the device rating of 1A. Please do check out the below application note to see various designs done to achieve various output voltage.
Signal and Power Isolation with 3.3 V / 5 V Input and 12 V / 15 V Output
For designing a transformer for custom voltages, please use the below transformer design tool.
Let me know if you have any further questions, thanks.
Regards,
Koteshwar Rao