Hi ISO team,
I saw the ISO1212 temperature rise picture shown in below from the ISO1212 datasheet in the first page.
We can see ISO1212 chip surface temperature is about 45°C.
May I know what the test condition is?
The Condition I mean is like that
" Input voltage is 60V or 24V? "
"What is the Current limit value?"
Thank!