Part Number: ISOUSB211
Hello TI experts,
my customer made their own PCB with ISOUSB211, and I asked some questions like below link ;
and they tested more with several different methods.
please see the picture below first.

at first they designed USB type C connector on downstream port because the module is connected by type c connector.
but they could not succeed with their PCB.
so they tried to change type C connector to type A (gray cable) -> using type A to type C cable (white cable) -> and finally connect the module. finally they succeeded with this configuration.
I don't understand that they used only USB 2.0 signals although they used type C connector. and I think there is no problem with it.
Could you check the schematic(in previous thread) and this method of connection again to solve this problem?
and I have another question, the temperature of ISOUSB211 goes up to 57 degree when it is working.(they used infrared thermometer) they feel very hot when they touch ISOUSB211.
is it normal situation?
(when they use power supply instead of USB 5V power, it consumes only 170mA.
if this kind of heat is normal, should I consider heat sync for cooling the device? or should we modify artwork for better cooling? (but I could not find thermal pad on ISOUSB211.)
please check these 2 issues. Thanks.
Best regards,
Chase