This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ISO7763DWR and ISO7763FDWR
Please tell me about the difference.
Also, ISO6763DWR is scheduled,
Is it okay to recognize that EN 61010-1 is certified?
I would like to adopt ISO6763DWR, but when will the certification be completed?
Since it is unknown, we are considering changing to ISO7763DWR.
The EN 61010-1 acquisition schedule for our equipment is tight.
Hi Takahashi-san,
Thanks for reaching out.
The only difference between ISO7763DWR and ISO7763FDWR is the default output state. ISO7763DWR has a default output state of HIGH while ISO7763FDWR has LOW output default state. Please refer to Table 1 and Table 2 in the datasheet, I am copying them below for your quick reference.
ISO6763 is currently going through the certification and soon will be certified. It has the same isolation technology as ISO7763, hence, we do not foresee any issues in ISO6763 certification. Thanks.
Regards,
Koteshwar Rao