Part Number: ISO7740
Other Parts Discussed in Thread: ISO7820
Hi,
Yes, we've already seen the TDDB plot and we will continue to discuss that, but idealy we need Failure Modes and Distribution with the item 'lost of isolation'. Is it possible for TI to provide this FMD: 'lost of isolation' of ISO7740, ISO7820... (double capacitive barrier devices)?
Inside 'slla508_iso7740' document there is also a note below the FMD table 3-1 where it is written 'The FMD in Table 3-1 excludes short circuit faults across the isolation barrier. Faults for short circuit across the isolation barrier can be excluded according to ISO 61800-5-2:2016 if the following requirements are fulfilled...'. The issue is that we don't have ISO 61800-5 yet.
Best regards,
Christophe