This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The TI ISO7740 isolator does not work properly, loses the signal, and the silionlab si8645ba can work properly. Please help analyze the reason
Note: the transmission is the pulse signal, the signal rate: 30MHz, the GND_F voltage variation amplitude -40V--0V, frequency: 50kHz
Hi Koteshwar,
The pulse width >10ns,
Look at the schematic diagram of my drawing. The first set of signals can be transmitted completely, but the three groups of signals are missing.
This problem should not be related to the pulse width.
Is it related to the negative voltage disturbance superimposed on the GND_F floating ground?
the pulse width>20ns,
the slew rate of this negative voltage disturbance: 50V/us
Vcc1: 3.3V Vcc2: 3.3V
it is being observed on multiple devices / PCBs