Part Number: ISO1540
Other Parts Discussed in Thread: ISO1640
Hi team:
can you help review the schematic for ISO1540?
The application is used Master to communicate with Hotswap controller (slave), but the reference ground is different.

During check DATASHEET recommend condition, we found Side1 IOL1 and IOL2 was proposal min is 0.5mA. and C1 Capacitive load side1 is 40pF max. which is not aligned with the schematic above. But we didn’t got fully understand why the recommended is like this, and how to calculated these. can you also help explain why we need to choose such value? Thanks