Part Number: ISOUSB211
Other Parts Discussed in Thread: AM2434, , ISOUSB111
Looking at implementing USB Isolation between an AM2434 (ALX) as a peripheral role and a USB2.0 connector.
Currently the part of choice is the TI ISOUSB211
It seems from the ISOUSB211 datasheet Figure 10.2 that the EQ configuration on peripheral application has a higher gain set on the MCU side than the connector side.
Q: I would have thought that the connector/cable end would need more gain than the couple of inches of track to the MCU. Why is this not the case here?
Q: The EQ setting is fixed, not dynamic. So how do you deal with different USB Cables?
Q: Given the LP-AM243X and its Tiny USB SDK as a starting point, if we wanted to remove the 480M capability so we can use a ISOUSB111 without 480M Support what is the right way to switch this off in firmware? (We don't really want to make a modified copy of the TinyUSB code and have to maintain it)
Thanks
Andy