This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO3088: DW0016B Footprint selection

Part Number: ISO3088


Hi,

              I have a design where I have been using the IC ISO3088DWR. Datasheets shows two footprints for DW package. What is the difference between them and which one should I prefer.(Note: I don't have any HV system on the other end and my usage is for isolation purpose.)

 

  • Hello Balakrishna, 

    Thank you for reaching out. The landing pattern on the left was introduced to comply with systems that have a >8mm clearance requirement (where clearance is the "line of sight" distance or the shortest air path between two conductors). 

    If 8mm clearance is not a requirement for your system and you have no HV concerns, then either land pattern will work.  

    Best,
    Andrew