This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
we are using this IC for our CAN network as improved design in our product but we are facing issues at site when multiple node (currently 24 nodes) connected.
This IC CAN H and L acros resistance value strat to reduce and cause whole CAN network colapse. we used to test our prototype with max 4 node with short distance no issue with 120ohm end resistor in end of network.
what cause CAN H to L resistance to drop after some times?. is it tranceiver wont support multiple node and long distance?. how to improve this resistance drop.
Can get contact number from technical support to come and take a look in our offcie.
Hello Latha,
Thanks for reaching out and for using ISO1042. The schematic is blurry, so I can't make out any details, however it looks like there are not any termination resistors used on the CAN bus. If the cable length between nodes is long this may also affect the maximum number of nodes the CAN bus can support as you suspected.
Please see 9.2.2.1 Bus Loading, Length and Number of Nodes. For a large CAN network with many nodes, bus parasitic often limit the maximum number of CAN nodes. Careful design and termination resistors can help extend the number of nodes supported (see 9.2.2.2 CAN Termination).
The following app not on CAN Physical Layer Requirements (ti.com) (Section 4) as well as Top Design Questions about Isolating CAN Nodes Bus Design (Rev. A) provide some good insights and on termination as bus characteristics as well.
Best,
Andrew
Hello Latha,
The amount of CAN nodes a bus can support is severely limited by cable lengths and signaling rate. The components marked with a red 'X' (and JP4 1-2 connected) are needed to for a split termination configuration. Operating without termination resistance (single or split) would be a possible reason the CAN bus is not communication.
The following snip taken from section 4 is also relevant if your application has a long stub length (>0.3m).
What is the cable length and signal rates for your application? Do you have scope captures from TXD and RXD to CANH and CANL?
Best,
Andrew
Hello Latha,
Two 120-ohm termination resistors shown above is sufficient. However, the "Good IC" looks like the CANH and CANL are not differential which suggests some error in the termination network. Please confirm that the second CANH and CANL captures are the same voltage-per-division on the scope.
Best,
Andrew
bad IC-CAN H and CAN L show voltage level upto 1.1 V and the wave form 200 microsec
Good IC- CAN H voltage level 3.5V and timing in 50 microsec and CAN L show Voltage level upto 1.1V and timing 50 micro
Hello Latha,
Based on the information provided so far, we have two concerns with the schematic:
From this we would recommend the following:
Best,
Andrew