Part Number: ISO7761
I am using ISO7761.
The data sheet states the following, but I think the actual operation is different from the description.
Attached is the circuit diagram and waveforms.


According to the data sheet, when VCCI is PD (<1.7V) and VCCO is PU (>2.25V), the output should be Default (High without F suffix).
However, according to the attached waveform, it looks like the Output is being driven low.

Q1:
What causes the behavior to differ from the datasheet?
Q2:
Is there a way to prevent Output from going L when VCCI is PD?
Pulling up Output with VCCO had no effect.
thank you.