Part Number: ISO1540
Other Parts Discussed in Thread: BQ76942
Hi Team,
Currently, customer used our ISO1540 meet some corner issue:
In customer system, he add a switvh(MOS) in the line of VCC, to turn-on and turn-off ISO1540, but at the time, SDA/SCL are always pulled-up by 3.3V. So the voltage stress of SDA/SCL will reach the corner when MOS turn-off(VCC=0V), which is shown as below, it is related to VCC volt.

So whether this case has risk in the system design? Whether SDA/SCL pin will damage due to the always pull-up power?
Any further questions please feel free to contact me. Thanks in advance.
BRs,
Francis