Other Parts Discussed in Thread: ISO7763, ISOW7843
Team,
1- Seeking for an Altenate for P/N ISO7741FDBQ with mirror orientation as per the image below on the right
The original P/N is with 3 to 5 pins as inputs and pin6 as an output and pins 12 to 14 as output and 11 as an input (as per image below on left side)
The Alternate should be the moirror image with pins 3 to 5 as outputs and pin6 as an input and pins 12 to 14 as inputs and 11 as an output (as per image below on right side)
Please note having the same P/N P/N ISO7741FDBQ and rotating it 180 degree on the board is not the solution for our design.
ie:
We had
The current configuration P/N ISO7741FDBQ is with 3 forward and 1reverse channels
We want
Configuration with 3 reverse channels and 1 forward channels
Your suport and fast reply is highly appreciated.
Thanks and best regards
Muna Al-Azzawe