Other Parts Discussed in Thread: SN6507, SN6507DGQEVM
I am trying to design a power supply using SN6507 with the following specification.
- Input – 8V to 16V
- Output Voltage – 15V
- Output Current ~20mA
I tried testing this concept using SN6507DGQEVM Evaluation board.
First step was to modify the transformer to a value which supports this requirement. For which I found the following reference :-
Considering the turns ratio of the above options I had to reverse(Primary <--> Secondary) the transformer present on the board i.e. Coilcraft TX1-ZB1459-BE.
Rds was calculated as per the following formula.:-
The slew rate and the frequency were kept the same. Output inductor bypass jumpers were removed.
The Testing result was disappointing, it had poor regulation. The PS doesn’t go into Duty cycle control for the required range of input.
Here the horizontal is the Vin and vertical is the Vout.
Can you figure out what can be issue? Let me know soon.