This electronic desing would be robust enough to withstand a very noisy 120 Vac line, with a 400/120 VAC three-phase transformer as its source. Connected in parallel on this 120 Vac line are the coils from the electric coupling contactors. It is highly susceptible to noise, arcing, spikes, and sudden voltage variations originating from the contactor coils, without deteriorating the ISO1211 inputs, and ensuring a constant output to the MCU for voltage presence detection.
*Gmov = Maximum AC Volts 140 V
I apologize for any mistakes, but the text was generated with Google Translate.