Part Number: ISO1644
Tool/software:
Hello,
Is there any concern with using 6-8 ISO1644 on the same I2C bus on the "1" side?
Thanks,
Bryan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO1644
Tool/software:
Hello,
Is there any concern with using 6-8 ISO1644 on the same I2C bus on the "1" side?
Thanks,
Bryan
Hello Bryan,
Thank you for reaching out. Side 1 is intended to have a direct and exclusive connection to the MCU; therefore, it is not recommended to connect side 1 nodes to the same I2C bus. For more information, please see [FAQ] ISO1640: Why are the maximum load capacitance and load current ratings for Side 1 of the ISO1640/ISO1641 less than Side 2?
Best,
Andrew