This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Dear Expert
I would like to ask a few questions about the application of the SN6507DGQR chip:
Application scenario, 12V input, output around 12V, transformer tie ratio 1:1,
1. To adjust the duty cycle, according to the specifications, it is necessary to increase the inductance. I have tested that the static power consumption is nearly 30mA. Without increasing the inductance, the static power consumption will be reduced by more than half, and the output will be more stable with the increase of load,
2. Can you provide a reference for the waveform of the switching frequency? The waveform I tested here is a square wave when the duty cycle is fixed at 50%, and the rest is an anisotropic wave
Hi Gabriel,
Thank you for reaching out. Please find my inputs below, thanks.
Regards,
Koteshwar Rao