Part Number: ISO7721
Tool/software:
Hi Expert,
For ISO7221x, if the VCC1=3.3V and VCC2=5V is possible in application?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO7721
Tool/software:
Hi Expert,
For ISO7221x, if the VCC1=3.3V and VCC2=5V is possible in application?

Hello,
Thank you for your question.
For ISO7221x, if the VCC1=3.3V and VCC2=5V is possible in application?
Yes, digital isolators can be supplied with different voltages within the recommended operating conditions on both sides of the device. Please check this FAQ for more details: [FAQ] Can I power the two sides of a digital isolator with different voltages? - Isolation forum - Isolation - TI E2E support forums
Regards,
Aaditya Vittal