Part Number: ISO1042
Tool/software:
Hi
The customer is expected to use the NVIDIA Jetson in the project. Which one do we recommend to use, ISO1042BDWVR or ISO1042DWVR? Or have other suggestions?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Gareth,
The only difference between ISO1042BDWVR and ISO1042DWVR is the isolation rating. The "B" version is for basic isolation and the "non-B" version is for reinforced isolation up to 10kVRMS Surge voltage. So it depends on whether the customer requires "reinforced" isolation specifically for the application. If so, then the ISO1042DWVR would be our recommendation.
Best,
Michael