Part Number: ISO1042
Other Parts Discussed in Thread: SN65HVD230, ISO7721, SN65HVD23
Tool/software:
Dear support,
i am quite confused about the topic and i ask for your support.
My schematic is stil DRAFT and i attach it here below:

On my board there is a microcontroller and i have two connectors for iso_CAN adn ESC_CAN: the first comes from a device which is referred to isoGND, the second one comes from a device referred to PGND and i need to isolate it from isoGND with ISO1042 device. Microcontroller need to communicate with both devices.
I am wondering if TXD and RXD can be shorted together as i did: can this cause any issue?
In addition, do i need to consider ESC_CAN as a different CAN bus from iso_CAN?
Thank you in advance.
BR,
Giorgio