This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISOW1412: ISOW14xx device for half-duplex

Part Number: ISOW1412
Other Parts Discussed in Thread: ISO1500,

Tool/software:

Hello team,

My customer is currently using Half-duplex RS-485 for their system, and they are interested in isolated RS-485 for some of the A/C models with many noise issues.

I introduced them ISO1500, but they were looking for a device with isolated power, so I hoped to promote our ISOW1412.However, I see that this device is a full-duplex device.

Do we have any half-duplex device with integrated isolated power?

If not, could customer still use this device? Or, should they use ISO1500 + Isolated DC/DC for half-duplex applications?

The reason why I hoped to introduce ISOW1412 was because customer's concern is that Isolated DC/DC would have switching noise..

Thank you in advance for your help.