Tool/software:
Hello,
I am using the SN6507 in an isolated DC-DC application and encountered unexpected behavior related to the CLK pin configuration.
Observed behavior:
- 
When I connect a 60 kΩ resistor from the CLK pin to GND, the SN6507 operates at ~200 kHz. 
- 
When I add a 1.2 V TVS diode (200 pF typical capacitance) between CLK and GND (in parallel with the resistor), the switching frequency increases to ~391 kHz. 
My questions:
- 
Does SN6507 monitor the CLK pin voltage or impedance at startup to decide how the internal oscillator should behave? 
- 
Is there any threshold voltage, pull current, or timing mechanism used internally that may be influenced by external RC components? 
- 
Why does adding a TVS increase the switching frequency significantly? 
- 
What’s the recommended way to configure the CLK pin if I want to rely on the internal oscillator but still provide some protection? 
This behavior is reproducible and consistent across samples.
Thank you for your insights!
Best regards,