Other Parts Discussed in Thread: ISO1450, ISOW1432
Tool/software:
Hi
I am looking to use the iso1452 device to isolate the microcontroller from the external rs485 bus. i am confused if i should use only the a and b output with a 120 ohm terminator resistor and an sm712 protection diode to the rs485 device. Do i need to wire also the y and z outputs ?
thanks
Jason