Tool/software:
Team,
I am looking into using an RC element as a low-cost timer to delay the startup of a fairly standard SN6505B setup. The delay does not need to be precise; the length just must be more than a certain minimum. From a prior post, I can tell that there is a 500kOhm pull-down resistor on EN (https://e2e.ti.com/support/isolation-group/isolation/f/isolation-forum/970077/sn6505b-q1-en-pin-pull-down-resistor).
Here are my questions:
1. During power-down, is there a potential for damage if the EN pin still has voltage on it after Vcc has already fallen to zero? This voltage would be from the RC timing capacitor; is there a maximum safe capacitance?
2. Does the SN6505B draw additional current when the EN pin is between the low and high positions? If so, how much? This is common on CMOS gates. I couldn't find a TI example, but I came across this graph on Nexperia's 74LVC1G17.
3. Does the SN6505B have a significant (>5uA) bias current on the EN pin other than the 500 kOhm pull-down current (which is predictable by modeling as a resistor)?