This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISOM8111: Ternary Output?

Part Number: ISOM8111
Other Parts Discussed in Thread: ISOM8110

Is there any way a single ISOM811x can output ternary states? For example:

-1, 0, +1

or

0, 1, high-impedance

  • Hi Johnny, 

    There is no option for ISOM811x to be used as "0, 1, High-Z" since it won't have a formal tri-state buffer. However, -1, 0, +1 may be possible using the ISOM8111 (or ISOM811(5-8) for bidirectional input). However, I think the answer will depend on what you need the output/control signal to be. I took a swing at simulating this using PSPICE for TI. 

    Below shows a simple operation where ISOM8110 will track the input signal and is decoupled using a series capacitor to get a +V or -V state. The input voltage will also match any intermediate state to match a 0-crossing. 

     

    Let me know if this is a good start or not. 

    Best,
    Andrew

  • Thanks for this! I just saw it.

  • Hello Johny, 

    Thanks for coming back. The ISOM8110 is designed to have a transistor output similar to a traditional BJT. This means that the part can be used in designs flexibly almost as a discrete. Please let me know if this was useful. 

    Best,
    Andrew