This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN6507: MAX output current under SN6507 push-pull isolation configuration

Part Number: SN6507

Hi,
Is it difficult to exceed 0.5A on output current under SN6507 push-pull isolation configuration?

My customer wants to implement the following. 

Input : 24V +-10%
Isolated Output : 24V
Isolated Output current : 550mA

Webench of SN6507 is only MAX 500mA current.  That is why I am asking.

Thanks and best regards,
M.Hattori.