Part Number: ISO7821
Other Parts Discussed in Thread: ISO7842
Hi,
Please provide documentation on the structure of ISO7821FDWW
1.Provide structural diagram of ISO7821FDWW
Datasheet (sllsem2f) We would like you to disclose such materials that you can see the structure of the
insulating part "SiO2 based Capacitive Isolation Barrier" shown in Figure11.
(structure of primary, secondary and secondary insulation).
In particular, the physical distance of Isolation Barrier is also required.
2.Offering "Reinforced Isolation Capacitor Life Time Projection for Devices"
Another device, ISO7842 data sheet page15 Figure1 and Figure2 shows the characteristics about lifetime and reliability due to insulation degradation.
Can you prepare the same data with ISO7821FDWW?
best regrads
cafain