This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1410: Will 3.3V or 5V supply influence the performance?

Part Number: ISO1410

Hi team,

Customer is using ISO1410B for their design but they only have 3.3V on board.

Will it lead to some disadvantage of communication distance/protocol/number of nodes or any other aspect?

Looking forward to your reply! Thank you!

Marc

  • Marc,

    Output differential voltage will be reduced for 3.3V vs 5V for Vcc2. This will impact communication distance(3.3V case will have smaller distance vs 5V). Also, the 3.3V transceivers should also still be compatible with any 5V transceivers that may be on the network.

    Respectfully,
    Lucas