Other Parts Discussed in Thread: ISOW7841, SN6501,
Hii,
I have a slight doubt of selection of Modbus Isolator
I have to isolate my signal as well as the power-
There are two options i am slecting among
1) ISO1410
in this i have to use separately Transformer Driver
2) ISO3086T
This has the transformer driver integrated in it
So which one to choose.
Apart from this, i would have aso used ISOW7841, but it is mentioned in a document that the efficiency reduces to 50%, what efficiency it is referring to.