Part Number: ISO3082
Other Parts Discussed in Thread: ISO1410
Hello:
ISO3082 has encountered some problems in use. I need your help.
1. Prepare to connect DE and RE# pin directly to AST2500 GPIO pin for control, I wonder if it is ok?
2. When R,D pin is connected to AST2500 RXD and TXD pin, do I need to exchange pin?
3. Can both VCC1 and VCC2 use 3.3v power?
Best Regards
Leon
文晔集团
广东省深圳市南山区高新中三道9号环球数码大厦12楼
Mobile:(86)159 8985 2994
Tel:(86)755-26743880 Ext:6643
Fax:(86)755-26743990