This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
It seems that the only difference is Withstanding isolation voltage. ISO7821 is 5700 VRMS, ISO7721 is 5000 VRMS. right?
Besides, for ISO7721 itself. DWV(8) package is 8.5mm clearance and creepage, DW(16) package is 8mm clearance and creepage. But their body size width are the same, why they have different clearance and creepage?
Hi Howard,
Along with current consumption per channel and package options, yes, the primary difference between the ISO7721 and ISO7821 is the isolation rating.
Please allow me to confirm some details regarding clearance and creepage parameters and follow up with you in 1 - 2 days.
Thank you for your time,
Manuel Chavez
Manuel,
Since VIOTM, VIOSM, VIORM are the same between ISO7721 and ISO7821 SOIC-16 DW package.
It seems that ISO7821 SOIC-16 DW package is not very competitive compared with ISO7721 regarding higher price. I haven't met a customer who only need higher Withstanding isolation voltage to 5700VRMS.
Can I conclude that regarding SOIC-16 DW package, I only need to promote ISO77xx?
Hi Howard,
The ISO7821 in either package may be chosen by customers with specific requirements and higher isolation voltage needs. Most customers find the ISO77xx devices to fit their requirements, so this part can be largely recommended. Please do confirm customer needs on a case-by-case basis and feel free to post on E2E in the future if there are any doubts.
The creepage and clearance differences between the ISO7721DWV and ISO7821DW come from the distance across the isolation barrier measured along the surface of the device, as shown in the image below. In this case, the difference between 8mm and 8.5mm is acceptable for customers trying to meet the same voltage ratings of both devices.
Thank you for posting to E2E,
Manuel Chavez