Other Parts Discussed in Thread: STRIKE
Hi Isolation experts,
When looking at section 7.2 of the ISO7741 datasheet - my customer is wondering if the ESD testing is performed when VCC1 and VCC2 are connected to power or is this test performed when there is no external power, just the ESD event?
Also, if it is different between JS-001, JESD22-C101, and IEC 61000-4-2 then please clarify the power state of each.
Thank you!!
Reed