Part Number: ISO3082
Other Parts Discussed in Thread: ISO1410
Hello , ISO3082 is a half duplex IC.
My doubt is:
1. If RE is connected to GND, then it is always in receive mode. Now if DE is also high. transmission will happen. Can transmission and receiving happen simultaneously in half duplex? Isn't it supposed to be one by one.
2. Do we need R132, R13 in the circuit ? If yes, why?
3. What is the purpose of R20 and R135? can we eliminate them?